4/22/2012 11:44 PM | |
Joined: 11/4/2011 Last visit: 12/8/2023 Posts: 253 Rating: (53) |
Well, I'm not that good expert to advise you 100% working solutions. But here it is, I've found information from PCS7 Compendium part A - Configuration:
I would reinstall Windows. Are you using SIMATIC IPC or usual PC? Cause IPC have Restore DVD – a good thing to reinstall whole system. I have several IPCs at the office for new project and at the first launch I should have entered PC name and I chose, for example, 00CWA91. But leading numbers should be avoided. So I renamed the stations to CWA91 etc. And I was working under my project having no access problems. However later I reinstalled Windows with Restore DVD just in case And check the user rights. Manual "PCS 7 - PC Configuration and Authorization", 4.4.7 Setting up user groups and users. Something remains in renamed PC's system... For example, the user group SQLServer2005MSSQLUser$<COMPUTERNAME>$WINCC containes the old PC name. Also I've got troubles when downloading project to OS Client (Windows XP) from ES Station (Windows Server). I should've been logged in as some new user (except Administrator) in OS and ES to be able to download a project. Do you think it's ok to have different versions of WinCC in one project? What version is installed on ES? I think that ES is creating OS projects for a specific version of WinCC that should not be open under other version. Am I wrong? |
4/26/2012 12:41 PM | |
Joined: 10/26/2011 Last visit: 4/17/2024 Posts: 763 Rating: (190) |
Hello I think, you have now PCS 7 V7.0 SP3... If that is right, you have to upgrade your older project(s) to the newer version. You cannot mix the versions. That will be the reasons of your error messages. Regards |
SIMATIC PCS 7 - Overview |
|
Follow us on