4/26/2012 12:55 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191) |
Hello I am confused. In the top, you wrote, that your new PC has PCS 7 V7.0 SP3 "Exising OS PC are having PCS7 V7.0 SP1 & WinCC V6.2 SP2 on Windows XP SP2, New OS PC is having PCS7 V7.0 SP3 & WinCC V6.2 SP3+HF1on Windows XP SP3."
|
SIMATIC PCS 7 - Overview |
|
4/26/2012 9:19 PM | |
Joined: 11/4/2011 Last visit: 8/25/2024 Posts: 253 Rating: (53) |
Excuse me, but haven't you forgot to Assign OS Server to the Client? Here are the documents that mention about a procedure: 1. PCS 7 Compendium Part A - Configuration Guidelines => 7.1 Project settings => 7.1.1 Defining the server assignment 2. PCS 7 - Configuration Manual Operator Station => 16.1.2 How to Download Server Data |
This contribution was helpful to1 thankful Users |
4/29/2012 2:20 PM | |
Posts: 691 Rating: (37) |
Hello Saravana kumar Are you able to access the Server from your New OS Client PC. Make sure that NewOS PC must connect to the Server at the Startup , It should not ask any login while accessing the Server |
This contribution was helpful to1 thankful Users |
4/29/2012 4:18 PM | |
Joined: 11/4/2011 Last visit: 8/25/2024 Posts: 253 Rating: (53) |
Sorry, what path are you opening? You mean Windows shared folder? |
Follow us on