12/19/2014 11:26 AM | |
Posts: 29 Rating: (0) |
Thanks Marcjan for your information. But one engineer came in site and told us that step7 V5.4 will not support this CP cards. |
12/20/2014 5:09 AM | |
Posts: 29 Rating: (0) |
Thanks. So I need GSD file for both card. Thanks Yaloo |
12/20/2014 3:02 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, You need a HSP ( Hardware Support Package) How can you update the hardware catalog without direct internet access? And this may be helpfull too. What should you watch out for when replacing the CP443-1 (6GK7443-1EX11-0XE0) with a CP443-1 (6GK7443-1EX20-0XE0 V1.0) in STEP 7 V5.4 SP3? Before trying this in the field, i would make a copy of the project and make the changes in the copy to see if everything compiles well. Regards, Marcjan |
Last edited by: Marcjan at: 12/20/2014 3:05 PMProblem solved? |
|
12/22/2014 1:15 PM | |
Posts: 29 Rating: (0) |
thanks |
12/27/2014 5:21 AM | |
Posts: 29 Rating: (0) |
Thanks you. I did same procedure as mansion in link and successfully set up communication with CP 443-1. But CP 443-5 (6GK7 443-5DX05-0XE0, Ver 7.1.) is not installed in HW because its’ need Sept7 Ver 5.5 SP1 but I have Step7 Ver 5.4 +SP5. Is it another procedure to communicate with CP 443-5 with Step7 5.4+SP5? |
3/17/2015 3:24 PM | |
Posts: 3 Rating: (0) |
Hello Yallo, Could you tell me where did you find the GSD download for 6gk7 443-5dx05-0xe0 V7.1 ?? I´m trying to find but without success.. Thank you. |
Follow us on