11/5/2014 12:28 PM | |
Posts: 6 Rating: (0) |
net |
Last edited by: masterec at: 11/5/2014 12:32 PM |
|
11/5/2014 12:29 PM | |
Posts: 6 Rating: (0) |
pg-pc |
11/5/2014 12:30 PM | |
Posts: 6 Rating: (0) |
ping |
11/5/2014 12:31 PM | |
Posts: 6 Rating: (0) |
s7 tool |
11/5/2014 4:05 PM | |
Joined: 7/7/2010 Last visit: 5/9/2024 Posts: 14701 Rating: (2355)
|
I am not an installation or software prerequisite expert, so you need to check whether the home premiums is supported for portal V13. If you already have update 5 installed, great. If not, installing it will not hurt. I notice your default system language was not German or English. When I see that and people have strange problems, I might suggest changing the portal default language to one of those (German or English) - whichever is closest to one they understand, and see if after changing the language if things magically work. Once resolved, please issue a Support Requestto alert Siemens HQ to the bug so they can fix it in future updates. Please post your results. Oh yes, did you install using "right-click, run as Administrator" when you installed portal? If not, you may need to uninstall and re-install. |
science guy |
|
11/5/2014 4:23 PM | |
Posts: 5225 Rating: (1187) |
I do not recommend to update TIA13 beyond update 4. Update 5 has got problems. [LINK] |
11/9/2014 5:49 PM | |
Posts: 6 Rating: (0) |
No, only shows s7usb, plcsim v5.x (PN.IE) and Teleservice
Tia Professional is not compatible but Tia basic is compatible
Yes is update
When I took the screenshots the language wasnt English but that was one of the things I tried I installed the software in a administrator user, I thought wasnt neccesary, I will tried this I would love to share results with you but I have urgency to finish the project I was working so I manage to change my laptop, If I come back to the problem laptop I post more results.
Ok I will try when I can |
Follow us on