9/11/2011 7:52 PM | |
Posts: 3 Rating: (0) |
hallo Splitted from No access to the SQL server. |
Last edited by: O_Moderator at: 9/12/2011 11:48 AMnew subject after splitting |
|
9/12/2011 4:08 AM | |
Joined: 5/19/2006 Last visit: 9/22/2024 Posts: 549 Rating: (107)
|
Did you check for any clues in WinCC Logs folder? Dec PS. Maybe you can attach in here those log files. |
9/13/2011 3:21 PM | |
Posts: 288 Rating: (22) |
You coould also check the status of the SQL Server WinCC Components in the SQL Server Configuration manager. If these are not running, force a start of all the services and try again. |
9/13/2011 8:33 PM | |
Joined: 1/17/2006 Last visit: 7/19/2024 Posts: 800 Rating: (63) |
Virusscanning? Active directory policy? Windows Patch? |
1/8/2014 11:48 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (41) |
Hi, have you tried to re- configure the PC Station in the SIMATIC Manager? Is your ethernetcard correct congifured in the SIMATIC Shell? advanced Networksettings (terminalbus on first place)?,... Regards, Healthcheck |
Grundkurs/Systemkurs WinCC V7: |
|
8/1/2014 12:35 PM | |
Joined: 6/4/2008 Last visit: 7/27/2024 Posts: 58 Rating: (1) |
dearWolfgang B i have faced same problem today itself & also solved it. You have to deactivate WinCC & then go to Alarm Logging. At there you will find Message archive option. Just right click it & reset the archive, After then restart PC & WinCC . Your problem is resolved. Thanks Jaydeep
|
This contribution was helpful to1 thankful Users |
9/23/2015 7:51 AM | |
Posts: 144 Rating: (7) |
Hello Same problem here. I am using pcs7 v7.0 (step7 5.4 wincc 6.2). The system was working ok but after a while same message appeared in Alarm Logging window. I reboot the system as recommended by the excel file of system messages and remedies .I also reset the archive. It works for sometime but the message raises again. New Alarms can be seen in Alarm logging window but they do not enter journal list and they are really lost! There is no entry in the files in Diagnose folder of Wincc related to this message. Has anyone solved this problem yet? |
Last edited by: r.ethernet at: 9/23/2015 7:54:23 AM |
|
Follow us on