12/1/2011 9:25 AM | |
Posts: 36 Rating: (2) |
Hello, I'm struggling with the horn. It's working excellent as long as I only compile and downlload an OS within Step 7 without writing 'single messages' via Excel interface (creating project folder, copying block 9&10 to message bit & tag in sheet 'single messages' etc). But this is neccessary since otherwise there won't be any 'W' 'A' or 'F' flasing on the faceplate indicating a warning, alarm etc. But as soon as I write the single messages and download the project again, the horn doesn"t work anymore, but why \ thx stefan My configuration: Microsoft Excel 2000 Microsoft SQL Server 2005 Siemens config is attached Attachmentused Siemens software.zip (70 Downloads) |
Last edited by: CS Moderator at: 12/1/2011 10:53 AMLast edited by: PackElend at: 12/1/2011 9:25 AM |
|
12/1/2011 11:29 AM | |
Posts: 1530 Rating: (59)
|
Hallo PackElend, could you please send an attachment of your Excel project map/alarm logging. Maybe something get in disorder? Waiting for your answer Bizur |
12/1/2011 3:05 PM | |
Posts: 36 Rating: (2) |
any way of emailing my project map, because I can't download anything it's 7mb large even tried splitted zip but still can't do it |
12/2/2011 5:02 AM | |
Posts: 36 Rating: (2) |
ok at least one part
Attachmentproject map OS1a.zip.002.zip (114 Downloads) |
12/2/2011 5:06 AM | |
Posts: 36 Rating: (2) |
and here the other part, hope u can unzip it. That's only the project map, do u need anything else? Attachmentproject map OS1a.zip.001.zip (105 Downloads) |
12/5/2011 10:15 AM | |
Posts: 1530 Rating: (59)
|
Hello PackElend, sorry, I have been a little bit too fast. Yes, for sure it works, if you cut the extension. Thank you very much Bizur |
Follow us on