3/9/2016 1:34 PM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
Hello, yes this is know. The problem is the graphic driver in the VM. If you use VMWare you must enable 3d Acceleration in the properties of the VM. If you use Oracle VM Virtualbox you must install the 3d Drives in the VM, you can read the steps to do here: https://support.industry.siemens.com/tf/ww/en/posts/141467/ .
Christoph |
Last edited by: ChristophD at: 3/9/2016 1:34:39 PMLast edited by: ChristophD at: 3/9/2016 1:37:04 PM |
|
This contribution was helpful to1 thankful Users |
3/9/2016 1:41 PM | |
Posts: 38 Rating: (0) |
Thank you for the answer! I'm using VMware workstation 12 player, and 3D acceleration is already enabled.. |
3/9/2016 2:13 PM | |
Posts: 38 Rating: (0) |
VMware tools are updated! I'm using an Intel I5 M560 CPU with integrated graphics. |
3/9/2016 3:05 PM | |
Posts: 38 Rating: (0) |
VMware SVGA 3D if I'm correct. Thank you for all the answers so far, I appreciate the support! |
3/9/2016 3:49 PM | |
Posts: 38 Rating: (0) |
The panel I use is a KTP700 basic; Tia portal V13 SP1 Update 7; WinCC advanced V13 SP1 Update 7; Windows 7 x64; |
Follow us on