8/30/2017 3:10 PM | |
Joined: 4/28/2015 Last visit: 4/21/2024 Posts: 578 Rating: (43) |
I tried that as well, ran into http://lists.openembedded.org/pipermail/openembedded-core/2017-June/137651.html and gave up with trying to work around this somehow after the feedback received from the community. There is much more work required. For now, it's better to install the node during runtime on the device than trying to package it with broken Yocto/OE. |
Last edited by: jan-k at: 8/30/2017 3:12:54 PM |
|
8/30/2017 9:40 PM | |
Joined: 4/28/2015 Last visit: 4/21/2024 Posts: 578 Rating: (43) |
In case of mass-rollout, I would recommend doing the install step once manually on one box and then replicate that image from the SD card. If you do the installation in a script similar to the disk expansion, make sure to specify the version you tested so that they are consistent across all devices. However, there is no infrastructure for such a script yet but inspiration can be found here: https://github.com/siemens/meta-iot2000/blob/master/meta-iot2000-example/recipes-example/iot2000setup/files/expandfs.sh. |
Follow us on