Industry Online Support
Technical Forum
10/26/2013 10:26 AM | |
Joined: 9/27/2006 Last visit: 1/17/2022 Posts: 62 Rating: (0) |
Hello This is the first project I have done with a non Siemens profibus device, in this case a Sabroe Unisab3 compressor controller. I have added the GSD file from Johnson Controls into the hardware configuration but would like a little bit of guidance regarding the telegram set up. I have added the GSD file and the Profibus manual to this email, any help will be appreciated. Regards Sean
AttachmentUnisab-III-1.08_Operating_en_2010-10.pdf (384 Downloads) |
10/26/2013 10:33 AM | |
Joined: 9/27/2006 Last visit: 1/17/2022 Posts: 62 Rating: (0) |
Hello Attached the profibus manual.
AttachmentUnisab-III_Profibus-Extended_2008-08.pdf (311 Downloads) |
Follow us on