2/8/2020 5:21 PM | |
Posts: 1 Rating: (0) |
We are using Wonderware 2014 in our works and Intouch data is available in KepServerex6. Want to transfer data to SQL data base using IDB 7.4. However when KepserverOPC is selected as Provider, I am not able to browse tags of the particular channel. However tags of Kepserver Simulator example are visible. As per IDB manuals, any OPC server can be selected as Provider. Can any one help me on this issue. However Kepserver OPC tags were visible to WinCC and as trial when the tags were logged in WinCC and WinCC OPC server was selected as Provider in IDB, it was able to browse all the tags. Wonderware, IDB, Kepserver are installed on same machine Any solution ? Regards ------------------------------------------------------------------------------------------ |
Last edited by: venkat0404 at: 02/08/2020 18:04:03Last edited by: venkat0404 at: 02/08/2020 18:07:23Last edited by: Jen_Moderator at: 02/10/2020 11:47:07New subject after splitting |
|
Follow us on