3/15/2021 7:38 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, Are you sure RNA version is released for PCS7? Normally the successor is 443-1EX30 |
If I could help you, you can use the RATE button. Thank you. |
|
3/17/2021 8:50 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
is it the netpro 4 ways communications you mean? CPU A Rack 0 to CPU B Rack 0, rack 0 ->Rack 1 , Rack 1-> Rack 0, Rack 1 -> Rack 1? Siemens remove this functionality from Step 7 V5.6 HF4. If you are using Step 7 V5.6 HF3, 4 ways of communication still valid. Once you updated to latest PCS7 release, HF4 and above, these connections will be gone. Siemens planned to put this functionality back in PCS 7 V9.1 SP1, which might be released in October 2021. Hope it is helpful for you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on