5/18/2009 8:01 AM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665)
|
Hello Fahaz; S7-PLCSim is not designed to simulate communication ports on the PLCs. It was designed to test the internal functions of your program, and it uses MPI to exchange data between the step 7 program and the simulated PLC in your computer.You cannot add Profibus or IE communications and communication blocks to the simulation. You can find other discussions of the same subject on the forum (use the search box at the top right and look for PLCSim, for example); one of these is located at this link. Hope this helps, Daniel Chartier |
9/2/2015 2:29 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665)
|
Hello; It seems that some members are still interested in the possibility of simulating communications between CPUs. In 2009, this was not possible using S7-PLCSim. The situation has evolved since, with upgrades to the software: How do you simulate communication between two CPU modules? Hope thuis helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on