10/28/2019 5:58 PM | |
Joined: 6/23/2008 Last visit: 4/17/2024 Posts: 1165 Rating: (279)
|
Hello mesnowball
Regarding this question have a look to this FAQ: Link Regards... |
"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
10/30/2019 1:23 PM | |
Joined: 8/22/2018 Last visit: 3/2/2021 Posts: 35 Rating: (0) |
Hi mark, Thanks, one question, if using plc Sim, still need to run OS simulation? Or can just click run button from here wincc explorer? Thanks regards, snowball
|
10/31/2019 8:31 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi snowball, the OS simulation is used in the engineering phase if you use OS Server with OS Clients. In this case you can't open WinCC Runtime from the Server on the ES and test something. These will lead to problems if you want to load and start later the Runtime on the OS Server. Therefor Siemens offers an FAQ What should you do if the OS server project is taken online by mistake on the ES?. More information about the OS simulation you can find in the manual SIMATIC Process control system PCS 7 Operator Station (V9.0 SP1) at section "Simulation of an OS". If you use a Single Station you don't need to use the OS Simulation, there you can always start the Runtime. With regards |
Last edited by: Heisenberg2 at: 10/31/2019 08:35:00 |
|
Follow us on