6/9/2011 1:39 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359) |
Section (10-14 to 10-19) of the following manual mainly discuss Master Control Relay in STL. http://support.automation.siemens.com/WW/view/en/18653496 Errors in programming or lack of full consideration while using MCR may cause CPU to stop . read these notes before using these set of instruction in your program. Also note this is not a good alternative for hardware emergency stop or safety system.
Check the attachment for more information. AttachmentMCR_NOTES2.pdf (491 Downloads) |
This contribution was helpful to2 thankful Users |
6/9/2011 2:52 PM | |
Posts: 2348 Rating: (263)
|
Thanks for the tip, hdhosseini [schnippschnapp] new question is splitted to the following thread Can anybody tell me when it''s more convenient to use MCR instead of standard methods?. |
Last edited by: O_Moderator at: 6/9/2011 2:56 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on