4/3/2014 7:21 PM | |
Posts: 8946 Rating: (999) |
I cant get your question... Please upload our script and explain what you want. |
4/8/2014 7:46 AM | |
Posts: 1299 Rating: (135)
|
Hello, in manual they recommend to use a bitwise comparison to analyze the return value of "GetAttr" K!ke |
4/8/2014 12:53 PM | |
Joined: 4/26/2012 Last visit: 4/26/2024 Posts: 1520 Rating: (158) |
OK, What I do not know, is that it is correct to do what I did in the example?? using "GetAttr" I tested Left ("teste01.txt", 4) and it returns me "test", but I can not list the existing files to see if there is one that starts on Archiving "test". The files are for example teste01.txt, teste02.txt, teste03.txt, no matter what exists after the fourth character on. Just want to know that there is at least one file that starts "test" thank you |
"Always make a backup before and check the best time before testing." |
|
4/9/2014 7:30 AM | |
Posts: 1299 Rating: (135)
|
Hello, what about creating one folder on usb where all "test..." files are stored and then analyzing if there are files in the folder or not? K!ke |
Follow us on