Industry Online Support
Technical Forum
1/20/2010 10:28 AM | |
Posts: 2930 Rating: (432)
|
Hi, I think this will help: http://support.automation.siemens.com/WW/view/en/14188898 Yes the TD works different then the OP. A TD change automatically from MPI to PPI if MPI is not possible. However, you can extend with an EM277 and use panles at the EM 277. I hope this helps |
1/20/2010 2:07 PM | |
Posts: 2 Rating: (0) |
Is there any configuration that has to be done in order to use EM277 for panel communication? |