6/1/2016 5:45 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, It is CUD1 card of 6RA70 DC drive. While placing order please mention number as C98043-A7001-L2 & provide complete drive MLFB number along with serial number. CUD1 is common card. Please refer attached sheet to compare terminal details with the card you want to order. HTH. Attachment6RA70 CUD1 .pdf (225 Downloads) |
9/22/2016 12:40 PM | |
Posts: 64 Rating: (0) |
Hi . I have two A7001-L2 board . one of them is A7001-L2 3 And the Other is A7001-L2 4 . I mean the last number 3 and 4 in the end of name board . A7001-L2 3 A7001-L2 4 Also you can see in the pictures attached . What is the different between two board ? Can I replace A7001-L2 4 whit A7001-L2 3 ? AttachmentA7001-L2.zip (184 Downloads) |
9/22/2016 1:46 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Please read below FAQ. XX It is latest software & data base for drive monitor. With these CUD cards you need latest drive monitor software which is not available for public. You need to contact your nearest Siemens service support for it. New Product Software V3.28 for SIMOREG DC Master / SIMOREG CM / SIMOTRAS HD for CUD1 electronics board version C98043-A7001-L2-xx |
Last edited by: PISCEAN 2010 at: 9/22/2016 1:49:12 PMLast edited by: PISCEAN 2010 at: 9/22/2016 2:11:02 PM |
|
9/22/2016 4:02 PM | |
Posts: 64 Rating: (0) |
Is there any problem if I replace A7001-L2 3 with A7001-L2 4 ? |
9/23/2016 5:30 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
No. You can replace. Only you need to check Drive monitor software version compatibility with the CUD |
9/23/2016 10:49 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Yes you can replace. |
Follow us on