1/24/2016 4:18 PM | |
Joined: 1/24/2012 Last visit: 3/2/2024 Posts: 34 Rating: (0) |
Operator forgets to turn off “test” switch resulting in Outputs remaining ON indefinitely. My solution is to replace the On/Off test switch with a momentary contact push button. Press once to activate 2 hour Off-Delay. Press again to cancel test. My problem…existing 0BA2 program uses 54 of 56 Function Blocks. My solution requires 3 additional FB. Before updating to a newer LOGO!, I wonder if there’s another solution. Normal 0 false false false EN-US X-NONE X-NONEAttachmentPushButton_Start_Stop.zip (211 Downloads) |
1/24/2016 4:46 PM | |
Joined: 1/24/2012 Last visit: 3/2/2024 Posts: 34 Rating: (0) |
Moments after posting, I discovered the solution! I guess I was "over thinking".?!? Anyway, thanks for looking. AttachmentPushButton_Start_Stop_V2.zip (232 Downloads) |
Follow us on