5/18/2012 10:00 AM | |
Posts: 87 Rating: (0) |
Dear Expert, Where I can get manual for old Simoreg 6RA2220-8DV70? I need to know about Analog Input characteristics. Thank you |
5/18/2012 10:41 AM | |
Joined: 8/25/2006 Last visit: 5/8/2024 Posts: 2203 Rating: (277) |
Hello. Manuals arehere. |
5/18/2012 10:53 AM | |
Posts: 87 Rating: (0) |
Dear KSN, Sorry I have got nothing manual at your link. Any one else? Many thanks. |
5/18/2012 11:17 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
hello, Mr. KSN is right. All manuals are available at the link. However please follow this. After opening the window just click on download. Since the manual size is greater then 3000 KB, couldn't attach it. Even if you are unable to get the manual, inform us so we could split the manual & attach here. For more information, please see the attachement. Hope this helps you. |
Last edited by: PISCEAN 2010 at: 5/18/2012 11:40 AM |
|
This contribution was helpful to1 thankful Users |
5/18/2012 11:38 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Please see this attachement. |
5/18/2012 11:42 AM | |
Joined: 8/25/2006 Last visit: 5/8/2024 Posts: 2203 Rating: (277) |
Ok. Directlink. Then follow the picture of PISCEAN 2010. |
1/29/2013 8:21 AM | |
Posts: 6 Rating: (2) |
Sasongkois right the manual on the link is for 6RA2220-8DV71 not 70! they are different |
1/29/2013 8:52 AM | |
Joined: 8/25/2006 Last visit: 5/8/2024 Posts: 2203 Rating: (277) |
It seems the difference is only in rated supply voltage 3AC 400V for DV71 and 3AC 380V for DV70.
|
Follow us on