2/5/2017 10:09 AM | |
Posts: 3 Rating: (0) |
Good day! I did not get to implement the delay on and off with the ability to pause/restart. In the attachment, attempting to use the generator and counter can't reset the counters after the completion of the working cycle. Should work like this: start (I3) on delay (with retentivity)- on - off delay (with retentivity)- readiness for the next cycle. I4 - pause/restart. Attachmenttimer test.zip (225 Downloads) |
2/5/2017 10:38 PM | |
Joined: 12/27/2006 Last visit: 4/15/2024 Posts: 1196 Rating: (113) |
If..... you use a a-sychronic pulsegenerator in combination with a counter then you have more flexibility to the programm. Make p.e. a pulsgenerator that make pulser every second. then you can count the pulses and make so your timer. With AND Blocks an OR blocks you can start, stop, pause en reset the timer on every state of your programm and give you the most fexibilyty Look in the attachment for a simple programm to use timers Attachmenttimer.zip (346 Downloads) |
Last edited by: Toeternietoe at: 2/6/2017 12:31:04 PM |
|
This contribution was helpful to1 thankful Users |
2/8/2017 12:20 PM | |
Posts: 3 Rating: (0) |
Toeternietoe, thank you.
|
Follow us on