10/2/2008 11:55 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hi My opinion is to use weekly timerwith combination with his FAQ: How do you switch over to summer or winter time in LOGO!Soft Comfort? regards |
10/2/2008 4:18 PM | |
Posts: 2930 Rating: (432)
|
Hi, if you want to generate the pulse, not based on a specific time/Date, why not using the puls generator? Regards Helmut |
10/2/2008 9:25 PM | |
Joined: 12/27/2006 Last visit: 4/27/2024 Posts: 1196 Rating: (113) |
Yes its possible. Look at the sample. I have made 2 samples. The first is the simplest. Block "Warte" is the waiting time for the firts power set-up. Do you need it?? AttachmentTimer-simpel.zip (236 Downloads) |
10/4/2008 7:15 PM | |
Posts: 2 Rating: (0) |
I have attached a program in LOGO SOFT which can be used for your application. Change parameters for T1 as 24 hrs and for T2 5minutes.I hope this will satisfy your application. Let me know
AttachmentLOGO!Soft Comfort - Timer circuit.pdf (255 Downloads) |
10/6/2008 4:25 AM | |
Posts: 241 Rating: (7) |
Hi cage, I THINK YOUR PDF FILE IS NOT COMPLETE..PLEASE RE-PRINT. |
10/18/2012 2:15 PM | |
Posts: 8 Rating: (0) |
Did you succeeded to solve this problem? |
Follow us on