5/20/2016 10:28 PM | |
Posts: 200 Rating: (6) |
|
5/21/2016 8:16 AM | |
Posts: 200 Rating: (6) |
zip attached
AttachmentAsh Manor.zip (90 Downloads) |
5/21/2016 9:37 AM | |
Posts: 5225 Rating: (1185) |
Andrew, I hoped I would understand what you want to do after seeing the project you sent. But I failed at that. I would think you would want to select between AUTO and MANUAL modes with F1 and F2. It does not make sense to me to have "while pressed" on there. I would expect "set bit" and "reset bit". F1 ... (a) set AUTO (b) reset MANUAL Also the SETPOINTS are bits where I expect to see VW word memory defined as INT data type. Regardless.... From what I understand what you ask, I have added some elements in your program. Note that I have added VW0 memory that is grouping bits V0.0 to V1.7 together as a unit. VW0 is then used to display a message. WARNING: Message 9 is linked to V0.1 and Message 0 is linked to V1.0. Pictures are also included to try and guide you further. w AttachmentProjectWithPics.zip (113 Downloads) |
5/24/2016 1:34 PM | |
Posts: 200 Rating: (6) |
When I press F2-F10 I get a message displaying the button that's been pressed when I press F1 I get no message |
Follow us on