5/31/2016 9:49 PM | |
Posts: 200 Rating: (6) |
Hi I have added a copy of the program. I have cut it down for this. I have added F1 and F2 and they are working with the logo fine. I have added what i think is the way to get the message as per some of the examples that have be given. So what i am trying to achieve is that a message will be shown when the relevant button has been pressed. When i do the the messages within the software all i get is a blank box on the screen. I am sure that when it has been shown i will be able to implement it to the other buttons. Thanks Andrew
AttachmentMESSAGES.zip (131 Downloads) |
6/1/2016 6:51 PM | |
Posts: 5225 Rating: (1185) |
Andrew, Thanks for the sample piece. There is background info that you need to know to make it work.. I have failed to demonstrate and tell you about that information. What really need is a tutor.. which I cannot be for you. Do think about visiting someone to give you a kick-start. Focussing on the functionality, attached is another design idea. It uses an internal variable as an indicator. Some notes follow. Consider simulating in this way: The tags were moved to new lists. Special attention to the single internal tag. A comment is also typed in the tag for you to read There are some objects on top of each other. All the objects are visible in the layers view. You can press the eye symbol to hide a layer of objects. The objects in Layer 2 are special and contain visibility animation settings. You will note that all the F buttons now have events. Inspect the differences among them. F1 and F2 has a different format than the rest. You can also inspect the changes in the text list. Simulate the HMI. The AUTO and MAN states changes as you press the F1 and F2 buttons. The text indicates which button is pressed. This does not give feedback (text message) if the PLC received the message or not. What are your thoughts? AttachmentMESSAGES_V2.zip (122 Downloads) |
6/6/2016 10:12 PM | |
Posts: 200 Rating: (6) |
Hi I have attached a copy of the program so far i have added some extra tags to the buttons and it works perfect thanks to the help given. Our emergency stop is controlled via a safety relay and follows all the guide lines for the safety circuits as this is the main core of our work installing safety systems. I have also added a text box that is hidden on the main screen and only becomes active from the estop healthy signal AttachmentMESSAGES_V3.zip (148 Downloads) |
This contribution was helpful to1 thankful Users |
6/6/2016 10:28 PM | |
Posts: 5225 Rating: (1185) |
Nice to hear you making progress!! There is some sample project about the password for you {here}. Cheers. |
Follow us on