3/5/2019 4:28 PM | |
Posts: 2 Rating: (0) |
Hi!
On second VM I have WinCC installed. I have changed VM`s IP to 10.67.143.10, in tag manager I set TCP/IP connection to 10.67.143.6...and it does not connect :( There is a connection between VMs, as I can ping first VM. What could go wrong? Is there any additional change to make in the second VM or in WinCC? Please write any ideas that come to mind. Thank you for any help!! d ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/6/2019 11:28:01 AMNew subject after splitting |
|
3/6/2019 10:49 AM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Hi If you want to use two computer , WinCC and PLCSIM, you can´t do it with PLCSIM, you need PLCSIM Advanced. It is spanish, but you can take a look to this |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on