5/13/2020 12:17 PM | |
Joined: 5/15/2019 Last visit: 3/21/2024 Posts: 18 Rating: (0) |
Dear Experts, I am using now iot2040,S7200 Smart Plc and communication between Node red to MindSphere. I have attached here all photos about problems and configuring, Even My problems are My mindsphere boarding status and online status is showing to me offline always. And Data Linked is also blank means no linked My configuration Of Mind sphere is 1st Opened ASSETS MANAGER Then Create Assets Type Next Aspects Then came to connectivity and Mind-connect Library. Please experts give me solution for this AttachmentMindsphere & node red.pptx (151 Downloads) |
I am very very thankful because of you friends are always with me |
|
5/14/2020 9:41 AM | |
Joined: 4/22/2016 Last visit: 4/11/2024 Posts: 25 Rating: (4) |
Hello Aditya, firstly pls update your Node-RED MindConnect Agent to the current version! I never work whit the RSA_3072, I prefer the SHARED_SECRET for connection testing. The benefit is you can easy copy the SHARED_SECRET key from Mindsphere to the node red MindConnect Agent! It is also not possible to connect the S7 node direct to the MindConnect Agent in node red. You need an function node where you define the dataPointId etc. from Mindsphere in a JSON Object. For more information pls check the following site chapter “Step 4: Create and deploy the flow Send data points” https://flows.nodered.org/node/@mindconnect/node-red-contrib-mindconnect I hope that is helpful for you |
This contribution was helpful to1 thankful Users |
Follow us on