8/3/2011 12:06 PM | |
Joined: 7/29/2009 Last visit: 10/20/2021 Posts: 16 Rating: (3) |
I just received a fix for the installation problems regarding S7DOS, which is responsible for the online interfaces. Unfortunatly I reinstalled my whole computer so I can't test the registry fix. Attached to this post is the fix Siemens mailed to me. Below are the original instruction that go along with the attachement. Perhaps any of you can test it and post the results here in this topic? Comments from Siemens: Our suggested workaround is as follow:
1. Unpack the attached ZIP file. 2. Rename the .re_ file too .reg 2.1 Maybe the content of the REG-File have to be changed to your situation (e.g. D: instead of C:)! 3. Start the .reg file with double click 4. Start a repair installation of Step7 V11. AttachmentS7DOS del reg if error 1605.zip (826 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on