10/6/2017 6:37 PM | |
Joined: 10/2/2017 Last visit: 12/8/2023 Posts: 25 Rating: (0) |
Hello, Murof. You are right. I would like to create with Pro Tool Pro an PC Runtime where the same project as on the OP can run and communicate with the PLC parallel to the OP. if it's possible in my case I'll appreciate any help. What do I need for it? I have all programmes on my laptop but something goes wrong and as a result, i get a problem. kindly find the attachment below. Attachmentscreenshots.zip (357 Downloads) |
Last edited by: Hamster74 at: 10/6/2017 6:43:53 PM |
|
10/9/2017 11:23 AM | |
Joined: 10/2/2017 Last visit: 12/8/2023 Posts: 25 Rating: (0) |
Hello, Wizard. Thanks for replying. I attached zip. file with the screenshots below. Could you retrieve it? Best regards. Hamster74 CPU-315-2 DP 6ES7 315-2AG10-0AB0 / V2.0 AttachmentDesktop.zip (317 Downloads) |
Last edited by: Hamster74 at: 10/9/2017 11:36:10 AM |
|
10/9/2017 12:13 PM | |
Joined: 10/2/2017 Last visit: 12/8/2023 Posts: 25 Rating: (0) |
hello, Wizard. Thanks for the advice. Unfortunately, I could do it only in a few days. Anyway, I will try to do it and, of course, I will let you know about the result. However, I have two more question. The first one: Am I right when I connect my laptop to PLC via that connector? (see zip.file below) The second question: Should I change any settings in Simatic ProTool or not? Best regards. Hamster74. Attachmentscreenshots.zip (286 Downloads) |
Last edited by: Hamster74 at: 10/9/2017 2:10:20 PM |
|
Follow us on