10/9/2021 9:29 AM | |
Joined: 3/28/2017 Last visit: 3/16/2024 Posts: 6 Rating: (0) |
Hello! I can't solve my problem. Some times I can't connect to my PLC 416-2 (6ES7 416-2XK04-0AB0, fw 4.0.2) with Step7 via TCP/IP. If I try to go online from any part of my program, I get message "Online: Connection could not be established. Connection partner not responding". When I repeat my attempts 10-20 times I sucsessfully go online. Also I open "Diagnostic" window only after many-many attempts... In my network there are about 10 PLCs with S7-400 CPUs, but I have trouble only with one. I try to increase "Cycle load due to communication" from 20% to 25% but this can't solve my problem. I attached diagnostic screens and buffer in zip-archive. Thanks for your help! AttachmentDiagnose.zip (166 Downloads) |
Last edited by: DMK_DIT at: 10/09/2021 09:29:52 |
|
10/21/2021 10:51 AM | |
Joined: 3/28/2017 Last visit: 3/16/2024 Posts: 6 Rating: (0) |
I still haven't solved my problem... |
11/3/2021 8:16 AM | |
Joined: 3/28/2017 Last visit: 3/16/2024 Posts: 6 Rating: (0) |
Please, advise at least in which direction to look for the problem... |
Follow us on