7/9/2013 3:29 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
It means your CFC program is different from the one online...Where CFC program is compiled to blocks. You have changed something in the offline program..It can also happen when for example you insert a VAT table...PCS7 checks the time stamp and it is different. Maybe you accidently did something to the CFC program, like adding, deleting an interconnection, inserted a new block You have to compile and download to get the problem solved.... |
If I could help you, you can use the RATE button. Thank you. |
|
7/10/2013 8:15 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
What do you do after download changes? Are you creating new VAT tables then? After download, your program should be consistent and you be able to go online, every significant change in CFC will result in a new download change... |
If I could help you, you can use the RATE button. Thank you. |
|
7/11/2013 4:58 PM | |
Posts: 836 Rating: (99)
|
can you try to use PLCSIM if there is the saem behavior |
Follow us on