7/5/2021 3:47 PM | |
Joined: 6/16/2016 Last visit: 2/29/2024 Posts: 15 Rating: (0) |
Hello, I have a new IOT2050 Advanced - 6ES76470BA001YA2. According to your explanation I understand that the IOT has OS pre-installed. When I turn on my IOT device, only the PWR LED lights up. The STAT LED turns on for a while / during device startup /, but then turns off, so only the PWR turns on. I have prepared a screen with DPP, I try to access login: root and password: root and I cannot access. The screen displays "Siemens Industrial OS 2.1.1 (based on Debian 10) localhost.localdomain tty1" Could you provide me with the username and password? Could you provide me the steps to follow to install the nodered? Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/06/2021 06:16:54New subject after splitting |
|
7/5/2021 4:52 PM | |
Joined: 6/16/2016 Last visit: 2/29/2024 Posts: 15 Rating: (0) |
Hi, If I have pressed the reset button for 10 seconds and it remains the same. Do you have any other ideas? |
7/5/2021 4:56 PM | |
Joined: 6/16/2016 Last visit: 2/29/2024 Posts: 15 Rating: (0) |
Hi Bergmanu, Another test.. I can ping, but I can't access from Putty
|