Industry Online Support
Technical Forum
6/24/2010 10:56 AM | |
Joined: 4/24/2006 Last visit: 9/23/2024 Posts: 8742 Rating: (1168)
|
Dear Vinny, For programming OP17 you will need Protool Lite or Protool or Protool Pro. Have a look here for transfer options: What transfer options are available in the various operator panels? Connection between OP17 and PLC is by using Profibus Cable and connectors. Best regards, Wizard |
6/24/2010 10:57 AM | |
Joined: 5/28/2008 Last visit: 9/21/2024 Posts: 4515 Rating: (839) |
Hello, OP17 software is Protool Pro. This FAQ will answer you about the type of connection you need for transfer the project to OP17. What transfer options are available in the various operator panels?
Please read the section14.2.3 Connections to PLC of this manual Hope this helps. |
Ayman Elotaify |
|
6/24/2010 11:01 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
Hello Vinny, Basically all you need is OP7, OP17 Operator Panel Cable for transfer/upload is Seriell RS232 (6XV1440-2K..) Info about this cable is there -What connecting cables are there for connections between the operator panels and the different controllers? Protool software for programming and Prosave software for backup. How to use Prosave - How do you backup/restore with a Windows-based panel? How to use Protool and make connection to the CPU - SIMATIC HMI ProTool How to configure text-based units Best regards, Hristo Mihalev |
6/24/2010 11:17 AM | |
Posts: 35 Rating: (0) |
Thanks everybody. Very helpful. |
Follow us on