Industry Online Support
Technical Forum
6/19/2008 3:54 PM | |
Posts: 5 Rating: (0) |
Dear ir We have tried replacing the cable as well, the problem still remains. |
6/19/2008 4:19 PM | |
Joined: 5/8/2006 Last visit: 2/14/2024 Posts: 1085 Rating: (77) |
Hi, if you use MPI or Profibus you can check theconnection in the PG/PC interface in the control panel of your PC. Bye |
6/20/2008 8:10 AM | |
Posts: 5 Rating: (0) |
Hi... Using profibus, connections checked. No result. What else could be wrong. In case OP is rebooting, what needs to be done?? |
6/20/2008 8:59 AM | |
Joined: 4/24/2006 Last visit: 4/15/2024 Posts: 8610 Rating: (1146) |
Hello, Did it all function before? What happened? Is interface area available in CPU? Best regards, Wizard |
6/20/2008 9:03 AM | |
Posts: 5 Rating: (0) |
Dear Sir The machine is a Hatebur Forging machine, working well for past 3 years. The problem started last week on it's on. We did not change any thing. Regards |
6/20/2008 9:28 AM | |
Posts: 5 Rating: (0) |
Dear Sir MPI address is already in program, Below message is shown when cable is disconnected: "PLC 2 adress not possible" Regards |
Follow us on