6/10/2014 1:47 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, Regards
André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster withinnovative PLC-Tools |
6/10/2014 2:20 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, where are you come from? You also can test a S5-cable for connection PG <--> S5. Please check your PM. Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster withinnovative PLC-Tools |
6/10/2014 8:35 PM | |
Posts: 784 Rating: (52) |
Hello, Design the cable in the attached file then use it. Press the keys ESC and Button up, when you power up the panel. (It will go into transfer mode) Best regards.....
AttachmentOP7.zip (475 Downloads) |
Last edited by: Wago at: 6/10/2014 9:07 PMProcessed transfer mode |
|
This contribution was helpful to1 thankful Users |
6/17/2014 12:26 PM | |
Joined: 9/11/2012 Last visit: 9/14/2023 Posts: 43 Rating: (0) |
Hello Ste39 Yes. The OP goes to READY FOR TRANSFER. The error message shows FUSE FAULT but no number. Ok. I checke the manual for System messages. It means this is not a system message. I dont the original project developed by the supplier of this system. But the problem is I cant get a backup. I have checked the communication parameters for serial comm is matching. Any suggestions? Regds Fredrick |
Last edited by: Fredrick D at: 6/17/2014 12:40 PMLast edited by: Fredrick D at: 6/17/2014 12:30 PM |
|
6/17/2014 1:26 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello Fredrick D, |
Last edited by: Ste39 at: 6/17/2014 2:55 PM |
|
This contribution was helpful to1 thankful Users |