3/7/2018 9:11 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147)
|
Hello tomi25, Please make sure you have unique MPI addresses for HMI and PC. Best regards, Wizard |
3/7/2018 1:35 PM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147)
|
Hello tomi25, Perhaps the following link might help: How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Best regards, Wizard |
3/7/2018 3:03 PM | |
Posts: 5 Rating: (0) |
Hi, My situation is while I reboot my OP I have a error "Change to operating mode online". OP manual suggest: ""Offline mode" and "Online mode" can be set on the configuration computer and on the HMI device. To set these modes on the HMI device, use a corresponding operator control object of the project." I assume I can't change 'online mode' on panel becouse there is no such option there. Since then I want to establish a communication between a PC and OP. Duris_I Yes, PG/PC and OP have different MPI addresses ( as You and Wizard suggested to change). Both PG/PC and OP have same MPI comm speed - 187.5 kbps Yes, you are correct. There is a cfg menu where I disable serial. On PC I checked box for PG/PC is only Master on network. I can't event be sure if program is there or not since "online mode" error. I can't use Profibus cable since I don't have a correct port on my PC (I only have male RS232 port) and also in pdf attached I don't see a option to connect to OP77B with Profibus cable. Wizard After creating this post I did follow this tutorial. Besides things You and Duris_I already point me out I stopped on point 5 where no network is detected on CP5512(AUTO). AttachmentPanels_Possibilities_of_connections.pdf (67 Downloads) |
Follow us on