5/21/2014 7:58 PM | |
Posts: 784 Rating: (52) |
Hello, Perhaps this thread might help: /tf/WW/en/Posts/108323#top Best regards.......... |
5/21/2014 8:07 PM | |
Posts: 784 Rating: (52) |
You need only the step for migrating WinCC Flexible into TIA Portal |
5/21/2014 8:16 PM | |
Posts: 165 Rating: (19) |
Hello, Kindly go through Migration WIncc Flexi to TIA V11 |
5/21/2014 10:51 PM | |
Joined: 5/28/2008 Last visit: 9/21/2024 Posts: 4515 Rating: (839) |
Hello, Did you see this tip: Hope this helps.
|
Ayman Elotaify |
|
10/11/2018 10:38 PM | |
Joined: 3/28/2015 Last visit: 8/25/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following manual might help: HMI devices Migration Guide Comfort Panel >>>> Part 3.3 Pages 27-35 "Switching screen from 4:3 to Wide screen" -------------------------------------------------------------------------------------------- The old HMI has a 4:3 display geometry and the new HMI has a 16:9 display. So it is possible after the migration the graphics in the screens are distorted. Before you do the migration, please look into the menu "Options -> Setting" in TIA. Here you can find the point "Visualization -> Resize Screen". Here you can do some changes/settings how the TIA-Portal will migrate different screen dimensions and resolutions. After you do these settings, you can try the migration. TIA is not a graphic program, which do rendering every pixel at a migration. --------------------------------------------------------------------------------------------- |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
Follow us on