3/10/2018 2:03 PM | |
Joined: 2/22/2018 Last visit: 10/27/2023 Posts: 2 Rating: (0) |
Hi, I'm trying to write into and read from an S7 using these nodes. My first node (a) is an OPC UA Item node with configuration
My second node with input from (a) is a OPC UA Client node with configuration
No I have an additonal OPC UA Client node with
As I set value in the Item to 30, I would expect the 30 to be write into the Tag of the S7, however, I get the error message:
This looks like a wrong data Type to me. Hence, I checked the Datatype in TIA and it is Int16. Also checked the Output of the Item using a Browse node, which generates
Thanks in advance for your help ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_7839215 at: 3/10/2018 2:05:05 PMformatting Last edited by: Jen_Moderator at: 3/12/2018 2:28:07 PMNew subject after splitting |
|
Follow us on