3/31/2017 9:55 AM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi,
try this! Afterwards it should work Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
4/5/2017 10:04 AM | |
Joined: 2/27/2014 Last visit: 4/19/2024 Posts: 689 Rating: (199) |
Hello, After updating to new OPCUA@0.2.11, i am facing some problem which is attached as video . Plz give ur suggestion. AttachmentIOT2040.zip (835 Downloads) |
With Best Regards, |
|
4/7/2017 6:24 AM | |
Joined: 2/27/2014 Last visit: 4/19/2024 Posts: 689 Rating: (199) |
Dear bergmanu, ID is 3 .Yesterday i did once again all configuration and now everything is working fine. Now my new task is to make IoT as OPC UA server, so i can connect with WinCC as OPC client to IoT. I need solution for two way communication (read and write) from PLC -IoT-WinCC and WinCC-IoT-PLC. I have successfully tested logo8!/S7200 SMART/S71200/S7300/S1500 over S7 communication with IoT and IBM cloud. S71500 OPC UA server communication with IoT to IBM cloud. S71200/S71500 Modbus TCP communication with IoT to IBM cloud. Now i need your help to make two way communication with our WinCC -IoT-PLC. |
With Best Regards, |
|
4/19/2017 2:59 PM | |
Posts: 69 Rating: (0) |
Is there a way to download the nodes and move them manually in the same directory. Does anyone have a download link for that? |
4/19/2017 3:10 PM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, if you go to https://flows.nodered.org/ and select the required node, there is always a link to github. There you can download the nodes as .zip file and copy the content of the .zip file to the directory. But I don't think this will work, because on this way no depencies will be resolved, which happens automatically by installing the node via npm. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
5/8/2017 11:10 AM | |
Posts: 69 Rating: (0) |
Page 7 mentions "Endpoint with IP address and port from the OPC UA Server" ... which is the right IP and Port? BR |
5/12/2017 7:55 AM | |
Posts: 215 Rating: (6) |
Can you show us your node configuration? I guess you're trying to read data from a PLC? What PLC are you using? How is it configured? |
5/12/2017 8:37 AM | |
Joined: 2/27/2014 Last visit: 4/19/2024 Posts: 689 Rating: (199) |
Hi, Have a look in attached screen shot and make necessary changes. AttachmentOPC UA.zip (852 Downloads) |
With Best Regards, |
|
Follow us on