7/30/2021 7:10 AM | |
Joined: 3/14/2008 Last visit: 5/6/2024 Posts: 2066 Rating: (928)
|
Hi, Yeah there is an easy fix. Make sure you set attribute: "Text 1" with the same name for SetOp and RstOp. In the faceplate only one of two commands is operable since the operation is determined by OS permission and a process release (Button can only be pressed if the interlock condition is ok for example). I do not understand why you (or customer) want to change it because as said, only one of two commands is operable. You have more functionality with separate buttons than with only one. Another option is to change the whole faceplate, add a script that will set SetOp and reset RstOp and vice versa when pressed again, but that is a lot of work.
|
Last edited by: Oreca at: 07/30/2021 07:12:05If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |