7/19/2007 8:16 PM | |
Posts: 3149 Rating: (171)
|
Hi which wincc version are you using? Is this happening with a new WinCC project as well? nemo |
7/19/2007 8:49 PM | |
Posts: 23 Rating: (1) |
WINCCClient is looking for an archive on C:\AffinerieAg\ArchiveManager\..... This is fine for the server but the client should search in \\SSC0018\AffinerieAg\ArchiveManager\... Where should I change this path?
|
7/23/2007 10:00 PM | |
Posts: 23 Rating: (1) |
WinCC V6.0 + SP 4 + Hotfix 2 |
Last edited by: Pacanins at: 23.07.2007 22:04 |
|
8/1/2007 12:47 PM | |
Joined: 7/18/2007 Last visit: 9/9/2009 Posts: 11 Rating: (0) |
I've got the same problem. But what's the solution? |
9/8/2007 4:34 AM | |
Posts: 2 Rating: (0) |
Dear All I am Also Facing The same Problem, Let Me know the Solution... |
3/12/2008 8:50 PM | |
Posts: 1 Rating: (1) |
Hi, do you use Simatic NET on your WinCC-server? Which versions? WinCC 6.0 is not compatible with Simatic NET V6.4. On the server the trends will work fine but on the clients you will get the message "load from archive ...". Even after deinstalation of SimaticNET V6.4 (Edition 2006) and installing SimaticNET V6.3(Edition 2005 HF1) the trends will not work on the clients. You will have to install Windows, WinCC V6.0 SP4 and Simatic NET v6.3 (Edition 2006 HF1). You can check the compatibility of WinCC and Simatic net on the WinCC V6.x Kompatibilitaetsliste: http://support.automation.siemens.com/WW/view/en/21927774 |
9/23/2008 11:02 PM | |
Posts: 23 Rating: (1) |
Yes, Thank you, that was the solution then. I forgot to come back to the forum and write the solution. Therewas something with the SIMATIC Net versions. |
Follow us on