11/27/2012 11:56 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Hello, pcs7 8.0 I have a custom block which calculates power consumption. In the mot_l block, I want to open faceplate with the SelFaceplate1 button. I connect this input with an output of the custom block. How does the faceplate open? How do I link the custom block to the faceplate? I already created the name: @PG_customblockname.pdl for the faceplate, but it is not working. Thanks! |
If I could help you, you can use the RATE button. Thank you. |
|
11/27/2012 5:12 PM | |
Posts: 836 Rating: (99)
|
Hi, did you create a APL like block for you custom block (Check APL Style Guide)? |
Last edited by: Silent Bob at: 11/27/2012 5:12 PM |
|
11/27/2012 5:28 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Ohh, Forgot to mention: Using APL library v8.0 |
If I could help you, you can use the RATE button. Thank you. |
|
11/28/2012 11:14 PM | |
Joined: 11/4/2011 Last visit: 12/8/2023 Posts: 253 Rating: (53) |
As far as I remember, it opens @PG_customblockname_standard.pdl – do you have that one ? I'll check it later |
11/28/2012 11:22 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Hello, I dont want to create a block icon... I want to open only a faceplate when pressing the faceplate button in the motor block (which is assigned to selfaceplate1 parameter) But I checked the name you applied terminalbuzz, I copied all faceplate pdl's and renamed to block name. Now it is working, so you have to get PG_customblockname_Standard picture. :) |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on