11/20/2015 7:54 AM | |
Joined: 7/7/2015 Last visit: 9/4/2023 Posts: 55 Rating: (0) |
Hi I Configured CPU315F-2PN/DP and ET200M and S110 in S7 H/W Station. But there are problem.... 2 day ago, I could click "start device tool" but, now it is locked.... yesterday, 'licence expire end' alarm appeared and then i opened licence. Is it related to licence? Do i format may computer? How I open STARTER by S7? Attachmentphoto.zip (254 Downloads) |
Last edited by: Ssung at: 11/20/2015 7:55:44 AM |
|
11/20/2015 8:46 AM | |
Joined: 7/7/2015 Last visit: 9/4/2023 Posts: 55 Rating: (0) |
Oh.. Thanks. I inserted SINAMIC station. and opened commissing. In this... I click, but alarm appeared. 1. Do i configure manaully s110 and motor? 2. Do i set PC/PG Interface again? STARER network cannot find CPU AND S110. Attachmentphoto2.zip (231 Downloads) |
11/20/2015 10:14 AM | |
Joined: 7/7/2015 Last visit: 9/4/2023 Posts: 55 Rating: (0) |
i tried to PROFINET IO -> Drives -> SINAMICS -> Sinamics S110 but, My CPU's BF2 and SF light. but, First i tried to GSD -> S110, no LED light. Is it PZD problem? -I didn't add more drive object. Attachmentphoto3.zip (251 Downloads) |
Last edited by: Ssung at: 11/20/2015 10:15:17 AMLast edited by: Ssung at: 11/20/2015 10:17:27 AM |
|
11/20/2015 10:24 AM | |
Joined: 5/12/2006 Last visit: 3/27/2024 Posts: 22162 Rating: (2962)
|
check the name of station of the device, the name mus onkine be the same like offline configured |
11/20/2015 10:24 AM | |
Joined: 7/7/2015 Last visit: 9/4/2023 Posts: 55 Rating: (0) |
Here is telegram status.. |
Follow us on