12/20/2016 11:28 AM | |
Joined: 12/16/2016 Last visit: 12/29/2021 Posts: 32 Rating: (1) |
Hello, my name is jeferson i from brazil. Here in my job have too many cpus 1200, but are they programmed with tia portal v11, and i have tia v13, so i can't upload it. I'm desperate, can anyone help? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/21/2016 12:39:40 PMNew subject after splitting Last edited by: Min_Moderator at: 12/21/2016 1:07:02 PMAdd links |
|
12/20/2016 11:46 AM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22228 Rating: (2980)
|
Hello, then try the following: create new project don't create a PLC expand in projecttree the Online Access go to the connected adapter and search for accessible nodes select the found pl then Menu Online -> Upload as new station to the project do this work or get you the same error? https://support.industry.siemens.com/cs/de/en/view/97554052
Christoph |
Last edited by: ChristophD at: 12/20/2016 11:48:01 AM |
|
12/20/2016 11:57 AM | |
Joined: 12/16/2016 Last visit: 12/29/2021 Posts: 32 Rating: (1) |
Please check if it's right. But i cannot upload because not appeare that option |
12/20/2016 11:58 AM | |
Joined: 12/16/2016 Last visit: 12/29/2021 Posts: 32 Rating: (1) |
oh man, i'm sorry. See it: |
Last edited by: jeffron at: 12/20/2016 11:59:41 AM |
|
12/21/2016 8:15 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello,
1-TIA V13 License can be used for TIA V11 or TIA V12 2-Download the trial Version of TIA V11 from Siemens Site. SIMATIC STEP 7 (TIA Portal) V11 SP2 TRIAL Download Hardware Support Packages (HSP) for WinCC (TIA Portal) V11 3-With TIA V13 license,you can obtain the full functional for TIA V11"Trial version". 4-You can install TIA V11 and TIA V13 together on the same PC. 5-Upload the program using TIA V11
|
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
Follow us on