Industry Online Support
Technical Forum
7/12/2010 3:55 PM | |
Posts: 6 Rating: (0) |
When I open the project for the first time, Scout says the project is a V3.1 project and needs to be converted. It seems to have no problem converting the project. I can open any STL or MCC program block with no problems notivced. I haven't tried opening the axex blocks or hardware blocks (drives, controllers, etc).. When I try to open or print previewa LAD program block, Scout crashes. I am uploading the project. the Siemens mail server requires that I split it into 3 pieces andI seem to only be able to attach 1 file at a time, so there will be 3 new emails with attachments of pieces of the file. Part 1 Attachment3206_041217a.zip (292 Downloads) |
7/12/2010 4:02 PM | |
Posts: 6 Rating: (0) |
I am uploading the project. the Siemens mail server requires that I split it into 3 pieces andI seem to only be able to attach 1 file at a time, so there will be 3 new emails with attachments of pieces of the file Part 2 you will need to delete the extension .zip from the file name so that the multipart zip will compile. the mail server made me add it on.
Attachment3206_041217a.z01.zip (261 Downloads) |
7/12/2010 4:05 PM | |
Posts: 6 Rating: (0) |
I am uploading the project. the Siemens mail server requires that I split it into 3 pieces andI seem to only be able to attach 1 file at a time, so there will be 3 new emails with attachments of pieces of the file Part3 you will need to delete the extension .zip from the file name so that the multipart zip will compile. the mail server made me add it on. the 3 files are 3206_041217a.zip, 3206_041217a.z01 3206_041217a.z02 Attachment3206_041217a.z02.zip (268 Downloads) |
Follow us on