2/26/2009 9:47 AM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
I am facing one problem with WinCC, on one day it will showing the following error (see the Attached file). after repair the WinCC the same problem remain, after reinstallation of OS (Windows XP Pro) & WinCC it works fine. so I am under stand it is problem of WinCC or My OS. AttachmentWincc.pdf (40 Downloads) |
Ammy |
|
2/26/2009 12:22 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hi Amit, did the error messages occur after reinstalling Windows and WinCC or did the messages come up again? Cumu |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
2/26/2009 12:52 PM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi Amit, WinCC installation and optional tools installation are same on both station? Regards |
Follow us on