2/27/2008 10:05 PM | |
Posts: 46 Rating: (1) |
Where have all the experts gone.... Any takers for this problem?!?!? Ragud |
2/28/2008 8:54 AM | |
Joined: 12/8/2006 Last visit: 11/27/2023 Posts: 170 Rating: (26) |
hiragud, ---------------------------------------------------------------------------------------------------------- (1) what is "step 7 symbol server" ---------------------------------------------------------------------------------------------------------- i have never used "step 7 symbol server" before. Are the "Step7 symbol server" and the "SIMATIC NET OPC Server" the same??? http://support.automation.siemens.com/WW/view/en/17413251 ---------------------------------------------------------------------------------------------------------- (2) Why do you have copy the wincc project to the other pc-station? ---------------------------------------------------------------------------------------------------------- (a) Do you use one engineering station for engineering Step7 and WinCC? (After "downloading" the WinCC-project to the other pc-station you can start the wincc runtime on the this pc-station.) (b) Do you want to make a really copy of the entire project (STEP7-project including winccproj)? ==> perhaps you should configure the pc station configurator again???? |
2/29/2008 5:08 PM | |
Posts: 46 Rating: (1) |
Thanks ateam, I'm gonna try that on monday to see if I get full funcionality back - I'll keep you posted Have nice weekend, Ragud |
Follow us on