1/30/2009 10:08 PM | |
Posts: 41 Rating: (1) |
Thank you bugmenot for your help! |
2/2/2009 12:13 PM | |
Posts: 31 Rating: (6) |
Hi. No problem mate! Just glad I could help someone for once bugmenot |
2/6/2009 1:57 PM | |
Posts: 31 Rating: (6) |
- Just download the package from the thread where I posted it (here). - Then extract "FunctionISALG_OperationLog.fct" to "C:\Program Files\Siemens\WinCC\aplib". - Open up "WinCC" and "Global Script C". - Click the "Generate Header" button and "SALG_OperationLog" should appear under "Standard functions". Open it and click "Compile and then "Save" - Open "Alarm Logging" and create a new "Single Message" and customize it like you want, but you can start by making it like I have in the screenshot I have attached in the .zip (make sure it is "Number" is 1001 like configured in the global script ("SALG_OperationLog"). - By now the script should be working if you have applied it to a button, but in case it is not follow the following steps: - Now extract "TestPicture2.PDL" into "C:\Program Files\Siemens\WinCC\WinCCProjects\***PROJECTNAME***" where ***PROJECTNAME*** is the name of your project. - Open "Graphic Editor" and "TestPicture2.PDL" and click "Run" to test wheter or not the script works. Please let me know if this works or not |