10/14/2015 2:22 PM | |
Joined: 10/9/2008 Last visit: 2/22/2023 Posts: 13 Rating: (0) |
Hi ; think that same topic was already traited but i still need some Help . Im using two siemens Motors in hoisting coupled regidly drived by two drive ( master slave ) 6RA7090 . communication are profibus between drive . setpoint and controle word1 by profibus . I try to do optimization P051 = 26 . i have r047 = 5 . i have see and read doc for simoreg and an application in internet " Master/Slave Switchover" . very helped . But i steel askink for : 1) How can i do in perfet condition ( by profibus or drive monitor .... see attached files .) making ON the optimisation . 2) i have read the following things by internet " The ramp-function generator and speed controller on the slaves are not active. When the drive is braked, all motors decelerate together along the deceleration ramp of the master and shut down simultaneously in response to n < n min) .How and with parametre to use for realizing that . thanks AttachmentPrametre list.zip (176 Downloads) |
Follow us on