8/21/2019 6:05 AM | |
Joined: 7/25/2017 Last visit: 4/21/2024 Posts: 295 Rating: (43) |
Regarding the statement in the S7-1200/1500 programming guide on optimized<->non-optimized data exchange: "For assignments with the same type between two tags with different memory I created a S7-1200 test program to compare copying between DBs of type UDT with optimized/non-optimized and ran it with 6000ms cycle time monitoring. The scenarios tested were:
The results are astounding - #2 was 10x faster than #1. See attached. AttachmentOptimized & non-optimized test.zip (73 Downloads) |
This contribution was helpful to4 thankful Users |
Follow us on