Industry Online Support
Technical Forum
8/26/2014 7:17 AM | |
Joined: 10/28/2008 Last visit: 7/21/2023 Posts: 245 Rating: (14) |
Hi. Please followdchartierreply. I think using IEC timers bring us advantages: 1) you can use as may timers as you need 2) it brings you advantage if you use timers inside function block. You can make it as multiple instance inside function block, so you do not have to "renumber" it if you use this function block several time. For example if you use function block for drive and inside this function block you have timers for fault of feedback of running drive evaluation. If you use IEC timer and make it multiple instance, you can call the function block of the drive and you do not have to care about renaming or renumbering of the timer in multiply call of the function block... Regards.
|
Georgio |
|