Industry Online Support
Technical Forum
2/16/2012 12:52 PM | |
Joined: 10/26/2011 Last visit: 5/3/2024 Posts: 761 Rating: (190) |
When a new version of PCS 7 is created the ability to order the media for previous versions is difficult. Need a link or part number for the older PCS 7 V7.1 SP1/2 DVDs. If PCS 7 V7.1 SP1 DVDs are needed order number S79220-B3026-F888 is available. If PCS 7 V7.1 SP2 DVDs are needed order number S79220-B3026-F888 will provide that installation DVD as well. Also need with the V7.1 SP2 update is order S79220-B2546-F888 to update the Step 7 license from V5.4 to V5.5 on the Engineering Station. This package will update up to 5 Engineering Stations. If PCS 7 V7.1 SP3 is being requested order number 6ES7658-4XX17-0YT8 is available. If this is not an update from V7.1 SP2 the following order is also needed S79220-B2546-F888 to update the Step 7 license from V5.4 to V5.5 on the Engineering Station. This package will update up to 5 Engineering Stations. S79220-B3026-F888, provides media for both PCS 7 V7.1 SP1 and SP2 as listed below: SIMATIC PCS 7, SOFTWARE SOFTWARE MEDIA PACKAGE V7.1 SP1, V7.1 SP2 SOFTWARE MEDIA WITHOUT LICENSE AUTHORIZED USE REQUIRES VALID LICENSE, R-SW, SW AND DOCU. ON DVD 5 LANGUAGES (G, E, F, I, S) EXECUTABLE UNDER XPPROF/ WINSRV2003 REFERENCE HW: PCS 7 547C: ES/OS, CLIENT, SERVER |
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to1 thankful Users |
Follow us on